Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

TPS-1 "192_168_16_210_upd.sts" File Not Generating

Last Updated:06/01/2017

Question:

The 192_168_16_210_upd.dat file was not generated automatically as indicated in the Getting Started Manual on pages 20-21. How do I get that file to generate?

Answer:

Please look in the document "TPS_Update_Manual_EN.pdf" located on the CD for the configuration of the TFTP server.
The TFTP response file "192_168_16_210_upd.sts" will be generated automatically in the "TFTP_Server_Dir" directory, when the download was performed. If you couldn't see the response file in the corresponding directory, this indicates that the download did not actually happen.
Suitable Products
TPS-1
  • Este artigo foi útil?