Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Is a 4.7 uF ceramic capacitor required the VDD15OUT pin of UPD720150?

Latest Updated:02/01/2009

Question:

Is a 4.7 uF ceramic capacitor required near the VDD15OUT pin of the UPD720150 USB host/peripheral controller?

Answer:

Yes, this capacitor is essential for satisfying the output specifications of the internal regulator. Be sure to place a 4.7 uF ceramic capacitor near the VDD15OUT pin.
Suitable Products
Serial Communication Controller