Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Explanation of Memory orderable part numbers

Latest Updated:10/05/2016

Question:

What is the difference between each part number?

Answer:

Please refer to the links in the below table which link to the appropriate page in the "explanation of orderable part numbers" document.

Please note that this table includes products regardless of status (mass production, non-promotion, others).

SRAM

EEPROM

Suitable Products
Memory