Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Which timing will extend if RAS is set up during CAS BFO RAS refreshment?

Latest Updated:03/23/2009

Question:

If RAS assert cycles are set up during CAS BFO RAS refreshment, which timing will be extended?

Answer:

SH7065=>TRrw is extended.

Except the above => the timing of TRc is extended.

Suitable Products
SH7065