Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What will initial value of the TxD pin be when TE bit of SCR is set to "1"?

Latest Updated:03/25/2009

Question:

When the TE bit of the serial control register(SCR) is set to "1" in serial transmission, what will the initial value of the TxD pin be?

Answer:

The initial value of the TxD pin will be the "High" level output both in Asynchronous serial communication and Synchronous modes, when the TE bit is set to "1".
Suitable Products
SH7144 Series
SH7080 Series
SH7060 Series
SH7065
SH7050 Series
SH7058
SH7055
SH7047 Series
SH7046 Series
SH7040 Series
SH7030 Series
SH7020 Series
SH7010 Series
SH7018
SH7011