Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What specification of synchronous DRAM do I have to confirm?

Latest Updated:03/23/2009

Question:

For the writing to mode register of synchronous DRAM after the power-on, the hardware manual says that which of X+H'FFFF0000 and X+H'FFFF8000 is used depends on the specifications of synchronous DRAM.  What specification of synchronous DRAM in particular do I have to confirm?

Answer:

Please confirm the following two points.

(1) The connection between SuperH microcomputer and synchronous DRAM.

  H'FFFF 0000 →SuperH microcomputer's A15 pin ="0"
  H'FFFF 8000 →SuperH microcomputer's A15 pin="1"

Please check to see if the A15 pin of SuperH microcomputer is connected to the synchronous DRAM.
If not, either address can be used.

(2) The mode register specification of synchronous DRAM.

For the mode register setting, it is necessary to use the address followed the mode register allocation of synchronous DRAM. Please confirm the correspondence of synchronous DRAM mode register bit connected to the A15 pin of SuperH microcomputer. 

Suitable Products
SH7616
SH7615