Pular para o conteúdo principal
Renesas Brasil - Knowledgebase

What procedure to get the (SDHI) on Section 18 in the hardware manual ?

Latest Updated:09/28/2009


What procedure does it need to get the SD Host Interface Specification (SDHI) on Section 18 in the hardware manual ?


For users of the SDHI on Renesas products such as the SH7671/SH7673 (SH7670 Series), SoC products, etc. , Renesas will confirm whether you have an SD Host/Ancillary Product License Agreement (HALA) with the SD Consortium, and then request an NDA for the disclosure of the SDHI specification for Renesas products. Please contact your Renesas sales agent about the NDA.
Suitable Products