Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What peripheral functions restricted when E10A-USB is used in SH7125?

Latest Updated:03/24/2009

Question:

What are the on-chip peripheral functions restricted when E10A-USB is used in SH7125?

Answer:

When E10A-USB is used, the function to show in the table below cannot be used because the function pins (H-UDI function pins) for E10A-USB of SH7125 is multiplexed with other function pins.

If E200F is combined with an evaluation chip unit and a user I/F board, pins are never occupied for the emulator use.

SH7125 Restricted Function Pins when using H-UDI function

Pin number H-UDI Restricted function
45 ASEBRK/ASEBRKAK FWE
32 TRST PA3/IRQ1/RXD1*1
31 TMS PA4/IRQ2/TXD1*1
28 TCK PA7/TCLKB/SCK2
27 TDI PA8/TCLKC/RXD2
26 TDO PA9/TCLKD/TXD2/POE8

Note *1: RXD1, TXD1 functions are output from the other pins.
      RXD1: 13-pin, 19-pin 
      TXD1: 12-pin, 18-pin

Suitable Products
SH7124, SH7125