Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What is the value of load connected with the D/A output pins?

Latest Updated:03/24/2009

Question:

What is the value of load connected with the D/A output pins?

Answer:

The absolute accuracy will be ±4LSB(max) when the load of D/A output pins is 2MΩ.
See the chapter of Electrical Characteristics of each products' hardware manuals for details.

The D/A output pin doesn't have the output buffer.
Because the value divided by resistor is output with switching a switch, please receive the D/A output with high impedance.

Suitable Products
SH7729R
SH7727
SH7720
SH7709S
SH7706