Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What is the recommended PAD diameter?

Latest Updated:09/28/2009

Question:

What is the recommended PAD diameter?

Answer:

Please refer to SH7619 Group Hardware manual's Appendix (C.Package Dimensions).
SH7619 ball pitch is 0.8 mm. So the recommended PAD diameter is showed as 0.35 mm to 0.45 mm.
Suitable Products
SH7619