Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What is suggested Pulse Transformer which is a RJ-45 connector type?

Latest Updated:09/28/2009

Question:

What is the recommended Pulse Transformer which is a RJ-45 connector separated type?

Answer:

S558-5999-46-F (BellFuse) has been tested on Renesas boards.
Suitable Products
SH7619