Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Should I output the read data from external to the end of the T2 cycle?

Latest Updated:03/23/2009

Question:

In the normal space accessing, although the specification of read data setup time 1(tRDS1) is provided from the end of T2 cycle, should I output the read data (output data from an external memory) to the end of the T2 cycle?

Answer:

It is not necessary for read data (output data from an external memory) to output to the end of T2 cycle.
The setup time is provided by tRDS1.
Please follow read data hold time 1(tRDH1) as hold time.
Suitable Products
SH7206