Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Is the data in the on-chip RAM retained at a reset?

Last Updated:10/18/2017

Question:

Is the data in the on-chip RAM retained at a reset?

Answer:

With the specified power supply, the data in the on-chip RAM is retained, regardless of a power-on/manual reset. However, if a power-on/manual reset is input during writing data to the on-chip RAM, the data in the on-chip RAM might be destroyed.
Suitable Products
SH7144, SH7145
SH7065
SH7058
SH7055
SH7050, SH7051
SH7052, SH7053, SH7054
SH7047, SH7049, SH7105, SH7107, SH7109
SH7046, SH7148, SH7101, SH7048, SH7104, SH7106, SH7108
SH7040, SH7041, SH7042, SH7043, SH7044, SH7045
SH7032, SH7034, SH7034B
SH7032
SH7020, SH7021
SH7018
SH7014, SH7016, SH7017
SH7011
SH7214, SH7216