Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Is it possible to connect SDRAM to CS2 and use CS3 space as a normal space?

Latest Updated:03/21/2012

Question:

The CS2 space and CS3 space are SDRAM connectable. Is it possible to connect the SDRAM to the CS2 space and use the CS3 space as a normal space?

Answer:

It is not possible to connect the SDRAM to the CS2 space and use the CS3 as a normal space.   

If you would like to connect the SDRAM to only one area, connect it to the CS3 space.

Suitable Products
SH7285, SH7286
SH7243
SH7214, SH7216
SH7231
SH7211
SH7083, SH7084, SH7085, SH7086