Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Is it possible to change the bit rate by the BRR using ASC?

Latest Updated:03/26/2009

Question:

If an external clock is used in Asynchronous serial communication, is it possible to change the bit rate by the bit rate register(BRR)?

Answer:

It is impossible to change the bit rate by the BRR, if an external clock is used. If the external clock is selected by setting the CKE bit of the serial control register(SCR), the bit rate will be the external clock divided by 16.
Suitable Products
SH7144, SH7145
SH7058
SH7055
SH7050, SH7051
SH7052, SH7053, SH7054
SH7047, SH7049, SH7105, SH7107, SH7109
SH7046, SH7148, SH7101, SH7048, SH7104, SH7106, SH7108
SH7040, SH7041, SH7042, SH7043, SH7044, SH7045
SH7032, SH7034, SH7034B
SH7020, SH7021
SH7018
SH7014, SH7016, SH7017