Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How to write the program in flash memory connected with the SuperH?

Latest Updated:03/23/2009

Question:

How should I write the program in the flash memory connected with the SuperH microcomputer?

Answer:

There is a method of using the emulator as a means to write the program in an external flash memory.
This is limited to the emulator with the function corresponding to writing in an external flash memory. Please refer to your manual of the emulator.
Suitable Products
SH7206
SH7619
SH7618
SH7616
SH7615
SH7146, SH7149
SH7144, SH7145
SH7083, SH7084, SH7085, SH7086
SH7047, SH7049, SH7105, SH7107, SH7109