Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How can I write programs in the flash memory connected to SuperH MCU?

Latest Updated:06/28/2011

Question:

How can I write programs in the flash memory connected to SuperH MCU?

Answer:

You have two options as described below.
1. Writing programs with an emulator with the function that supports writing to an external flash memory. Please check the specification of your emulator.
When you use Renesas Electronics E10A-USB emulator, please refer to “Flash Memory Download Program Application Note for E10A-USB Emulator”.
You can download the document from the following web site.
http://www.renesas.com/products/tools/emulation_debugging/onchip_debuggers/e10ausb/child_folder/e10a_usb_flashmemory.jsp

2. Writing programs with a flash memory writing tool.
Suitable Products
SH7730
SH7723
SH7722
SH7760
SH7751R
SH7751
SH7750S
SH7750R
SH7729R
SH7727
SH7721
SH7720
SH7709S
SH7706
SH7705
SH7286
SH7285
SH7263
SH7261
SH7243
SH7211
SH7206
SH7203
SH7201
SH7146, SH7149
SH7131, SH7132, SH7136, SH7137
SH7083, SH7084, SH7085, SH7086