Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Can SH7705 TRST pin (142-pin) be pulled down? (In normal operation)

Latest Updated:09/10/2007

Question:

Can SH7705 TRST pin (142-pin) be pulled down? (In normal operation)

Answer:

TRST pin can be pulled down.

Since the internal pull-up MOS is turned ON, small amount of current flows when TRST pin is pulled down externally.

It results in no damage to chip reliability.

A following process can stop this small amount of current.

The normal operation starts after the power-on reset.
Then, PTG3 of the Pin Function Controller can be set Port input (pull-up MOS: Off) with PG3MD1=1,PG3MD0=1.

Suitable Products
SH7705