Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Can I rewrite TIOR to switch rising and falling edge while timer is on?

Latest Updated:03/26/2009

Question:

As for MTU2(Multi function timer pulse unit 2), is it possible to rewrite the timer I/O control register(TIOR) to switch rising edge and falling edge of input capture input pins while the timer counter is counting.

Answer:

Do not change timer I/O control register (TIOR) while timer counter is counting.
Suitable Products
SH7206
SH7124, SH7125
SH7146, SH7149
SH7083, SH7084, SH7085, SH7086