Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What power supply is required for RZ/G1?

Latest Updated:12/02/2015

Question:

What power supply is required for RZ/G1?

Answer:

The necessary power supplies are as follows.

1.8 V: ETM, SD, LVCMOS I/F, Xtal, JTAG, Trace and RST
1.03 V: core, SATA, PCIe, USB 3.0
1.5 V or 1.35 V: DDR3-I/O or DDR3L-I/O
3.3 V: Others

Suitable Products
RZ/G1E
RZ/G1M