Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What formats are supported by the SD card interface?

Latest Updated:12/02/2015

Question:

What formats are supported by the SD card interface?

Answer:

SD, SDHC, and SDXC are supported. However, CPRM is not supported. In terms of physical specifications, interface 0 supports SDR104 and interface 1/2 supports SDR50.
Suitable Products
RZ/G1E
RZ/G1M
  • Este artigo foi útil?