Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

RZ/T1 Pin State During Resets

Last Updated:09/27/2017

Question:

What is the state of the pins during a reset?

Answer:

Except for the RSTOUT# pin, ERROROUT# pin and the XTAL pin, all pins are in the Hi-Z state.
Suitable Products
RZ/T1
  • Este artigo foi útil?