Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

5V Tolerance for All Functions on Shared Port

Last Updated:09/27/2017

Question:

If a port is 5V tolerant, does that tolerance apply to all functions shared on the port? 

Answer:

Yes, it does. 
Note that when VCCQ33 is less than 3.0V, the rated value of 5V tolerant ports becomes 3.6V.
Suitable Products
RZ/T1