Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Why does an error occur when I write to the user boot area?

Latest Updated:01/23/2014

Question:

Why does an error occur when I write to the user boot area?

Answer:

The device is shipped with the USB boot program written into the user boot area. If the user boot area is not erased prior to programming, a write error occurs.
Suitable Products
RX630
RX63N, RX631