Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What is the device code in device information sent by the boot program?

Latest Updated:05/20/2014

Question:

When the "supported device inquiry" command described in the ROM (or Flash Memory) chapter of the user's manual: hardware is used, what is the "device code" in the device information sent by the boot program?

Answer:

(RX610/RX621/RX62N/RX62G/RX62T)
It is 4 bytes of data showing information concerning the devices supported by the boot program.
Please use it using the "device selection" command.

(RX630/RX63N/RX631/RX63T/RX210/RX21A/RX220/RX110/RX111)
It is 4 bytes of data showing information concerning the devices supported by the boot program.
It also shows the endian (little endian or big endian) of the data to be programmed to the on-chip flash memory.
Please use it using the "device selection" command.

Suitable Products
RX62N, RX621
RX62T
RX610
RX62G
RX630
RX63N, RX631
RX63T
RX210
RX21A
RX220
RX110
RX111