Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What is single write strobe mode appears in Buses chapter in manual?

Latest Updated:06/20/2013

Question:

What is the single write strobe mode that appears in the Buses chapter of the hardware manual?

Answer:

Single write strobe mode selects which control signals are used when accessing external memory (16bits width).  It is defined in Section 11.3.3 of the HW manual.
Suitable Products
RX62N, RX621
RX610
RX63T