Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Requirements for industrial applications performed by the new RX65N/RX651 MCU

Last Updated:11/13/2017

Question:

What are the requirements for industrial applications?Can the new RX65N/RX651 MCU perform the requirements?

Answer:

Compared with other IoT devices, industrial applications are designed for long-term operation, which involves unique and sometimes challenging requirements, such as firmware updates in the field. The new RX65N/RX651 MCUs feature dual bank flash integration supporting both BGO (Back Ground operation) and the SWAP function, making it easier for system and network control manufacturers to execute in-the-field firmware updates securely and reliably.
Suitable Products
RX65N, RX651