Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

PHY-LSI to Ethernet Controller PCB Design Guide

Last Updated:08/25/2017

Question:

I need to connect the PHY-LSI externally to an ethernet controller. Is there any reference material to help with circuit board design?

Answer:

Visit the Renesas website and see the application note ”Ethernet Hardware Design Guide (r01an3342)” for board design assistance when connecting to the Ethernet PHY-LSI.
Suitable Products
RX64M
RX71M