Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

M3S-T4-Tiny TCP/IP Stack - SSL/TLS and IPv6 Capability

Last Updated:06/08/2017

Question:

Does M3S-T4-Tiny (Renesas' TCP/IP protocol stack software) support SSL/TLS encryption communication or IPv6?

Answer:

M3S-T4-Tiny does not support these items.

For more advanced communication functions, please consider other TCP/IP options by third party vendors.

More information, please refer to the specifications found on the M3S-T4-Tiny web site.
Suitable Products
RX62N
RX63N
RX65N
RX64M
RX71M