Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Is the only use of general-purpose register R0 as a stack pointer?

Latest Updated:06/20/2013

Question:

Is the only use of general-purpose register R0 as a stack pointer?

Answer:

Basically, R0 is used as a stack pointer.

There are two types of stack pointer. The stack pointer select bit (U) of the processor status word (PSW) is used to select which stack pointer R0 is used as.

However, in a situation when neither interrupts nor subroutines are used, it is possible to use R0 as a general-purpose register that uses the same addressing mode as another general-purpose register.

 

Suitable Products
RX62N, RX621
RX62T
RX610
RX630
RX63N, RX631
RX210
RX220
RX110
RX111