Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Is the FRDY bit set to 1 when an error occurs during programming of ROM?

Latest Updated:01/23/2014

Question:

Is the FRDY bit set to 1 when an error occurs during programming/erasure of ROM (flash memory for code storage)?

Answer:

Yes. The FRDY bit is set to 1.
Suitable Products
RX630
RX63N, RX631
RX210