Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How to operate the sub-clock?

Latest Updated:05/27/2013

Question:

The sub-clock won't operate.

Answer:

Please perform the following handling when using the sub-clock.
- Attach a sub-clock resonator
- Set the sub-clock oscillator stop bit (SOSCCR.SOSTP) to 0 (sub-clock oscillator operates)

 

Suitable Products
RX62N, RX621