Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How do I receive using the RSPI?

Latest Updated:12/18/2013

Question:

I want to receive using the RSPI, but I don't see a receive mode. How do I receive?

Answer:

To receive using the RSPI, set to transmit/receive mode and perform dummy transmission (data will be shifted out).
Suitable Products
RX62N, RX621
RX62T
RX62G
RX630
RX63N, RX631
RX63T
RX210