Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Expanded functions of the RX65N/RX651 lineup

Last Updated:11/13/2017

Question:

What kind of functions are installed in the expanded lineup of RX65N/RX651?

Answer:

The expanded lineup features MCUs with integrated Trusted Security IP (TSIP), and enhanced, trusted flash functionality and human-machine interface (HMI) for industrial and network control systems.
Suitable Products
RX65N, RX651