Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Can I access using a size that hasn't been enabled?

Latest Updated:06/20/2013

Question:

There are access sizes specified in the I/O registers. Can I access using a size that hasn't been enabled?

Answer:

Using Access sizes that are not specified in the I/O registers will not read/write correctly. Please use access sizes that are specified.
The "I/O Registers" chapter of the hardware manual contains information on internal register addresses and bit configuration. Please refer to the section on your peripheral module for details.
Suitable Products
RX62N, RX621
RX62T
RX610
RX62G
RX630
RX63N, RX631
RX63T
RX210
RX220
RX110
RX111