Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

A single write strobe mode in Buses chapter of User Manual: Hardware?

Latest Updated:01/23/2014

Question:

What is single write strobe mode in the Buses chapter of the User's Manual: Hardware?

Answer:

For the RX Family, the mode in which there is a single write signal and the valid byte position is specified by the byte control signal is called single write strobe mode.

In contrast to this, the mode which doesn't use the byte control signal and uses multiple write signals is called byte strobe mode.

Suitable Products
RX630
RX63N, RX631
RX210