Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Why do the LEDs connected to ports light upon reset? How can I prevent it?

Last Updated:12/26/2017

Question:

The LEDs connected to the ports light upon reset. What is the cause and how can I prevent it?

Answer:

Upon reset, except for some, all the ports are in a high-impedance status.
When TTL is used for the external buffer, there is a high likelihood that the high-impedance status will be judged as a high level.
If the circuit is designed so that LEDs light when the port outputs are high level, the LEDs will light as a result.

The handling to prevent this is to make the LEDs light when a low level is output.

Suitable Products
RL78 Family
78K Family