Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What is the error of the clock used for the timer, etc.?

Latest Updated:12/01/2011

Question:

What is the error of the clock used for the timer, etc.?

Answer:

There is no error between the internally generated clock based on fxx and the calculated value.
If there is an error, it is caused by the variation of the oscillation clock (main system clock).

Now, judging from the contents of your inquiry, what you are describing is more likely to be a timer interrupt variation rather than a clock error.
The timer interrupt variation is the variation that occurs in the interval from interrupt occurrence until the start of processing, and varies between 7 and 32 clocks depending on the instruction that is currently being executed.
(It's also based on the relationship with the other interrupts. The interval is even longer if the status is the interrupt disabled state.)

Suitable Products
RL78 Family
78K Family