Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What are set/reset conditions for INTAD interrupt flag for uPD780058?

Latest Updated:12/01/2011

Question:

What are the set/reset conditions for the INTAD interrupt flag for the uPD780058?

Answer:

Set occurs when A/D conversion ends or when setting is performed by software.
Reset occurs when the CPU is reset, when clearing by software is performed, or when the INTAD interrupt is acknowledged by the CPU.
Suitable Products
RL78 Family
78K0/Dx
78K0/Fx
78K0/Ix
78K0/Kx
78K0/Lx
UPD78F07xx
UPD7800xx
UPD7802xx
UPD7803xx
UPD7807xx
UPD7808xx
UPD7809xx
UPD780xx
UPD78F8025
78K0/VAN ASCP