Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Is there a sample program for clearing/starting the watchdog timer?

Last Updated:12/26/2017

Question:

Is there a sample program for clearing/starting the watchdog timer?

Answer:

No, there is no such sample program.
The watchdog timer is a function used to detect an inadvertent program loop, and should therefore always be cleared while the program is operating normally.
The practical usage of watchdog timer differs depending on the system, so there is no sample program.
Suitable Products
RL78 Family
78K Family