Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Can PSW ID flag control be performed and operate by the user?

Latest Updated:12/01/2011

Question:

Can PSW ID flag control be performed by the user?
Is a system call provided to operate the PSW ID flag?

Answer:

This is managed by the OS. Do not manipulate this within the OS.
Suitable Products