Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Which case is oftenly used in L level H level and high impedance result?

Latest Updated:12/01/2011

Question:

If a microcontroller port is damaged, I believe that there are cases when the L level, H level, and high impedance result, but which case is the most frequent?

Answer:

This depends on the usage method, so it is not possible to tell which case is the most frequent.
Suitable Products
RL78 Family
78K Family
  • Este artigo foi útil?