Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Protocol stack memory size

Last Updated:02/13/2017

Question:

How much memory does the protocol stack consume?

Answer:

For an estimate of how much memory is consumed by the protocol stack in the RL78/G1D, refer to the table below.
Measurement conditions: Protocol Stack V1.20, CC-RL v1.03.00, The number of connected slave is 1 unit
* Please calculate only the profile roles to be used.

●    The Embedded configuration

                                                   ROM (bytes) RAM (bytes)
Core Stack 108,277 7,769
Profiles Find Me Profile (FMP) Target 666 15
Locator 941 28
Proximity Profile (PXP)  Reporter 860 17
Monitor 1,838 52
Health Thermometer Profile (HTP) Thermometer 2,072 58
Collector 3,259 114
Blood Pressure Profile (BLP) Sensor 1,740 62
Collector 2,755 102
HID over GATT Profile (HOGP) HID Device 4,273 322
Boot Host 3,986 74
Report Host 5,425 106
Scan Parameters Profile (ScPP) Server 1,073 24
Client 1,493 46
Heart Rate Profile (HRP) Sensor 1,650 66
Collector 2,686 100
Cycling Speed and Cadence Profile (CSCP) Sensor 2,102 71
Collector 3,106 108
Cycling Power Profile (CPP) Sensor 4,265 126
Collector 4,715 164
Glucose Profile (GLP) Sensor 2,811 119
Collector 3,783 110
Time Profile (TIP) Server 1,513 45
Client 2,425 74
Running Speed and Cadence Profile (RSCP) Sensor 2,096 54
Collector 3,026 108
Alert Notification Profile (ANP) Server 1,533 44
Client 2,203 60
Phone Alert Status Profile (PASP) Server 1,324 25
Client 1,992 48
Location and Navigation Profile (LNP) Sensor 4,148 118
Collector 4,241 126
Profile Common (Service) 1,128 52


●    The Modem configuration

                                                   ROM (bytes) RAM (bytes)
Core Stack 116,891 9,048
Profiles Find Me Profile (FMP) Target 781 15
Locator 1,135 28
Proximity Profile (PXP)  Reporter 1,019 17
Monitor 2,081 52
Health Thermometer Profile (HTP) Thermometer 2,327 58
Collector 3,536 114
Blood Pressure Profile (BLP) Sensor 1,961 62
Collector 3,006 102
HID over GATT Profile (HOGP) HID Device 4,623 324
Boot Host 4,544 80
Report Host 6,056 112
Scan Parameters Profile (ScPP) Server 1,294 24
Client 1,720 46
Heart Rate Profile (HRP) Sensor 1,857 66
Collector 2,947 100
Cycling Speed and Cadence Profile (CSCP) Sensor 2,361 71
Collector 3,384 108
Cycling Power Profile (CPP) Sensor 4,623 126
Collector 5,021 164
Glucose Profile (GLP) Sensor 3,097 119
Collector 4,072 110
Time Profile (TIP) Server 1,770 45
Client 2,692 74
Running Speed and Cadence Profile (RSCP) Sensor 2,355 54
Collector 3,304 108
Alert Notification Profile (ANP) Server 1,792 44
Client 2,475 60
Phone Alert Status Profile (PASP) Server 1,582 25
Client 2,265 48
Location and Navigation Profile (LNP) Sensor 4,483 118
Collector 4,547 126
Profile Common (Service) 1,129 52
Suitable Products
RL78/G1D
Bluetooth