Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Maximum number of registered paired devices

Last Updated:02/13/2017

Question:

How many paired devices can be registered?

Answer:

Paired device information is saved in the data flash. Therefore, the number of devices that can be registered depends on the available capacity of the data flash.
Suitable Products
RL78/G1D
Bluetooth