Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Limit on number of mode transition of the Adaptable Function

Last Updated:02/13/2017

Question:

Is there a limit on the number of the Adaptable Function mode transitions within a certain period for the RL78/G1D?

Answer:

There is no limit on the number of transitions.
The mode automatically transitions with the RSSI value at that time (Low Power ⇔ Normal ⇔ High Performance).
The Adaptable Function is effective only when slave connection is active.
Suitable Products
RL78/G1D
Bluetooth