Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Applications of program Flash ROM 128KB model

Last Updated:02/13/2017

Question:

What applications can fit into the 128KB program flash memory?

Answer:

Applications that use Beacon or small memory profiles (FMP, PXP, etc.) can fit by using a code efficient compiler like CC-RL.
Suitable Products
RL78/G1D
Bluetooth
  • Este artigo foi útil?