Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Bluetooth Specification Version of Product Implementing RL78/G1D

Last Updated:02/05/2018

Question:

What is the Bluetooth specification version of a product that implements the RL78/G1D or RL78/G1D module (RY7011)?

Answer:

The Bluetooth specification version of the end product is "4.2" as the core specification version supported by the core (protocol) stack, installed in the RL78/G1D and RL78/G1D module (RY7011), is applied.
Details of core stack can be confirmed with Launch Studio of Bluetooth SIG below.
https://launchstudio.bluetooth.com/ListingDetails/10444
Suitable Products
RL78/G1D
Bluetooth