Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Warning Markers Shown despite No Build Errors_e² studio

Last Updated:12/20/2017

Question:

Even with no build errors, syntax errors and warning markers are shown in e² studio Editor and Project Explorer views.

Answer:

Codan (CDT static code analyzer) shows those errors and markers based on database generated by Indexer. Indexer would skip crawling symbol definitions upon running out of Indexer buffer.  In that situation, skipped symbols will be detected as unresolved. This issue can be solved by increasing the buffer size by the following 

Visit "Window" menu -> "Properties", then open tree "C/C++" -> "Indexer".
You will see the following dialog:
indexer_bufsize_en.png
Please set larger values for both "Skip files larger than" and "Skip included files larger than". Then, build the project or rebuild the index.

Note: Compiler specific definitions that are not described in any header files are recognized as unresolved symbols.
  Please refer to the following FAQ page for the solution.
How to suppress "Type '***' could not be resolved" code analysis error?

Suitable Products

e² studio
  • Este artigo foi útil?