Pular para o conteúdo principal
Renesas Brasil - Knowledgebase

Error message: CC-RX compiler V. 2 L2330 section address out of range

Latest Updated:10/29/2014


When I use the CC-RX compiler V. 1, it produces the following error message. What should I do about it ?

L2330 (E) Relocation size overflow : "file name.obj"-"section name"-"00000025"


This message is output if the branch width from "file name.obj" will be illegal.

  • If you are using the High-performance Embedded Workshop:
    In [RX Standard Toolchain], click on the [Details] button on the [CPU] tabbed page and change [Width of divergence of function] to [32 bit] (the default setting is [24 bit]).

  • If you are using CubeSuite+:
    In [Property] of the CC-RX (build tool), change the setting on the [Common Options] tabbed page to [CPU] -> [Branch width size] -> [Not specified (-branch=32)] (the default setting is [Compiles within 24 bits (-branch=24)]).
Suitable Products
CS+ (formerly CubeSuite+)
High-performance Embedded Workshop

C/C++ Compiler Package for RX Family1