Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Can run-time routine in a function be counted as the number of cycles?

Latest Updated:09/10/2007

Question:

Can run-time routine called by performance analysis in a function be counted as the number of cycles?

Answer:

Including a run-time routine, none of functions called in functrion is counted.
Suitable Products
High-performance Embedded Workshop
Simulator Debugger for SuperH Family [for High-performance Embedded Workshop]
Simulator Debugger for H8SX, H8S, and H8 Families [for High-performance Embedded Workshop]